NSK wants to offer its clients what is best in the market. To do that, it combines its competence in products and services to that of its partners, which have high reliability in the industry. Converted in one of the solid service pillars of NSK, the Training department keeps up with the new technological trends, and grows each day.
The Tradeshows and Workshops are two update and refresh modes in the Maintenance Function.








NSK Brazil Continues Strong Growth
NSK will nationalize line for industry imported from Japan.
Car manufacturers expect a 5% to 6% growth next year
See the list of NSK Distributors throughout the Brazilian territory.

NSKNET
Training Portal
Esfera NSK Magazine
 
© 2008 NSK Brasil Ltda. All rights reserved | Use Terms
  • Português
  • Español